I have just obtained an answer from application team. I am sharing how it is:
“From a voltage robustness perspective, just for the K31X/K32X and K34X parts allow up to 5.5V on V15.
However, for an application using more than 1.5V, the max die temperature Tj must be analyzed as MANDATORY. The max die temperature must not reach values beyond +150oC.
It is a matter of effective thermal resistance, run current of the application and input voltage where it ends up.
In my opinion, the V15_extended range is not recommendable for medium-High temperature applications.
I'm working to add these considerations and limitations in the new version of the DS”