S32K344-Secure Boot Software

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K344-Secure Boot Software

跳至解决方案
1,137 次查看
Simon-Liu
Contributor V

Hello

I am using the S32K344 EVB board for development work. I would like to implement the secure boot function. Is there any example?

 

BestRegards,

Simon

0 项奖励
回复
1 解答
1,115 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Simon,

I suggest you take a look at the example in S32K3 MCUs for General Purpose HSE Demo Examples (S32K3_HSE_DemoExamples)

S32K3_HSE_DemoExamples Secure_Boot examples.jpg


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,116 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Simon,

I suggest you take a look at the example in S32K3 MCUs for General Purpose HSE Demo Examples (S32K3_HSE_DemoExamples)

S32K3_HSE_DemoExamples Secure_Boot examples.jpg


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

785 次查看
yumi
Contributor II

Hi Robin, I tried to transplant SHE SecureBoot example from the S32K344 HSE Demo Examples to S32K312,  but when I debug , at the end of ConfigureSHESecureBoot, the smrCoreStatus_Get

as below, but after reset(icon as below), the code can't run to AppBL, so what should I pay attention when I transplant?

yumi_0-1742288685577.png

yumi_1-1742288746888.png

标记 (1)
0 项奖励
回复