S32K344-Pins supported by the CLKOUT_STANDBY function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344-Pins supported by the CLKOUT_STANDBY function

ソリューションへジャンプ
2,240件の閲覧回数
Simon-Liu
Contributor V

Hello

In the [Chip clock outputs] section of RM, there are the following notes:
What does [CLKOUT across functional reset and standby is supported only on GPIO[12]] mean? Does it mean that only GPIO[12] can output clock during functional reset and standby?

SimonLiu_0-1735279026365.png

 

BestRegards,

Simon

0 件の賞賛
返信
1 解決策
2,218件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Simon-Liu ,

   Thank you for your interest in the NXP S32K product, I would like to provide service for you!

    It means, to functional reset + standby, the CLKOUT function just works on GPIO[12], you can consider, GPIO[138] can't support it the function reset+standby at the same time, it should just works on the standby mode.

 

Wish it helps you!

Best Regards,

kerry

元の投稿で解決策を見る

2 返答(返信)
2,219件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Simon-Liu ,

   Thank you for your interest in the NXP S32K product, I would like to provide service for you!

    It means, to functional reset + standby, the CLKOUT function just works on GPIO[12], you can consider, GPIO[138] can't support it the function reset+standby at the same time, it should just works on the standby mode.

 

Wish it helps you!

Best Regards,

kerry

2,187件の閲覧回数
Simon-Liu
Contributor V

Hi @kerryzhou 

Thank you for your answer.

I understand that if a functional reset occurs, GPIO[138] cannot output the clock.

 

BestRegards,

Simon

0 件の賞賛
返信