S32K344 MCAL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
37,904件の閲覧回数
jacst
Contributor II

Hello, I am using S32 DS to configure the S32K344 EVB program. Can I use the configuration tool to configure the PORT and clock module, and then use the MCAL of this tool to configure other peripherals? For example, CAN, DIO
Because the configuration interface of this tool is more friendly, but we need to use AUTOSAR, can we use it in combination?

0 件の賞賛
返信
1 解決策
37,887件の閲覧回数
hungnguyenphi
NXP Employee
NXP Employee

Hello @jacst ,

 

Yes, use can use the configuration to to config Port and clock module. But user also need to configure the MCU MCAL configuration because other modules (Eg: can) get the reference clock value from MCU module.

hungnguyenphi_0-1633318231254.png

 

 

Best regards,

Hung

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
37,888件の閲覧回数
hungnguyenphi
NXP Employee
NXP Employee

Hello @jacst ,

 

Yes, use can use the configuration to to config Port and clock module. But user also need to configure the MCU MCAL configuration because other modules (Eg: can) get the reference clock value from MCU module.

hungnguyenphi_0-1633318231254.png

 

 

Best regards,

Hung

0 件の賞賛
返信