S32K344 MCAL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 MCAL

Jump to solution
37,902 Views
jacst
Contributor II

Hello, I am using S32 DS to configure the S32K344 EVB program. Can I use the configuration tool to configure the PORT and clock module, and then use the MCAL of this tool to configure other peripherals? For example, CAN, DIO
Because the configuration interface of this tool is more friendly, but we need to use AUTOSAR, can we use it in combination?

0 Kudos
Reply
1 Solution
37,885 Views
hungnguyenphi
NXP Employee
NXP Employee

Hello @jacst ,

 

Yes, use can use the configuration to to config Port and clock module. But user also need to configure the MCU MCAL configuration because other modules (Eg: can) get the reference clock value from MCU module.

hungnguyenphi_0-1633318231254.png

 

 

Best regards,

Hung

View solution in original post

0 Kudos
Reply
1 Reply
37,886 Views
hungnguyenphi
NXP Employee
NXP Employee

Hello @jacst ,

 

Yes, use can use the configuration to to config Port and clock module. But user also need to configure the MCU MCAL configuration because other modules (Eg: can) get the reference clock value from MCU module.

hungnguyenphi_0-1633318231254.png

 

 

Best regards,

Hung

0 Kudos
Reply