Hello NXP team!
I need some assistance in order to find a work around the BCTU CL max ADC channel size. Can anyone suggest me something here ?!
I loved the BCTU approach because it fully disengages the CPU from the ADC conversion. But I never until now have noticed that the BCTU's CL has mas size of 32 ADC channels.
Kind regards,
kyf
Solved! Go to Solution.
Hi,
if different ADC channels are going to be converted you can try to simply create chain of normal or injected conversions on ADC module directly.
BR, Petr
Hello @PetrS .
Thank you for reaching out !
max 32 commands can be configured in conversion list CL. This cannot be extended.
I've figured this out, what I'm asking here is, if there is a way to do this functionality without the BCTU.
Regards,
kyf
Hi,
if different ADC channels are going to be converted you can try to simply create chain of normal or injected conversions on ADC module directly.
BR, Petr
Hi,
max 32 commands can be configured in conversion list CL. This cannot be extended.
BR, Petr