S32K344 - How to trigger ADC conversion at the center of OPWMCB ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344 - How to trigger ADC conversion at the center of OPWMCB ?

ソリューションへジャンプ
1,629件の閲覧回数
kyf
Contributor V

Hello all !

I'm studying how the OPWMCB mode of eMIOS channel works in order to set-up a center aligned PWM output. I've seen that the only Flag generation that OPWMCB mode is in the trailing or both trailing-leading edges of PWM pulse but instead of this I need flag at bus over/underflow.

I need to trigger my ADC conversions at the points that are shown in the image bellow:  

center aligned pwm.jpeg

Does anyone know if it is possible to trigger an ADC conversion with BCTU at the time shown in the image ?

 

 

Kind regards,

kyf

0 件の賞賛
返信
1 解決策
1,598件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

in OPWMCB mode you need to select the timebase using Bus Select (Cn[BSL]). The timebase you select must be running in Up Count-Down Count mode and this timebase define PWM period. The channel generating this timebase can be then used to trigger ADC conversions at middle and period boundary. 
See MCB mode description to know more about flag generation in MCB Up Count-Down Count mode.

BR, Petr

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,599件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

in OPWMCB mode you need to select the timebase using Bus Select (Cn[BSL]). The timebase you select must be running in Up Count-Down Count mode and this timebase define PWM period. The channel generating this timebase can be then used to trigger ADC conversions at middle and period boundary. 
See MCB mode description to know more about flag generation in MCB Up Count-Down Count mode.

BR, Petr

0 件の賞賛
返信