S32K344 - FreeRTOS Build Errors from example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 - FreeRTOS Build Errors from example

Jump to solution
930 Views
DiaDev
Contributor III

Hello!

I am currently working on a FreeRTOS project for S32K344, and I'm facing some issues with the build configuration. I have attached an image for reference.

Platform: S32DS for platform 3.5
FreeRTOS Package: SW32K3_FreeRTOS_11.1.0_5.0.0_CD1_D2409_DesignStudio_updatesite
Thank you in advance.

DiaDev_0-1745317735343.png

 

 

0 Kudos
Reply
1 Solution
893 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Did you follow the chapter 2.2 Installation Design Studio of SW32K3_FreeRTOS_11.1.0_5.0.0_CD1_D2409_ReleaseNotes.pdf?

Make sure S32 Design Studio v3.5.13, S32 Design Studio for S32 Platform v3.5.13 with support for S32K3XXdevices (com.nxp.s32ds.s32k3xx.update_3.5.13.20240726235844.zip, com.nxp.s32ds.s32k396.update_3.5.13.20240726233621.zip and com.nxp.s32ds.update_3.5.13.20240726233529.zip ) and RTD package (SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410_DesignStudio_updatesite.zip ) are installed before this FreeRTOS package.
The S32K3XX RTD update for Design Studio must be installed as the following steps:
• Open Help -> S32DS Extensions and Updates. From the next windows, select "S32K3 Real-Time Drivers AUTOSAR 4.7 R21-11 Version 5.0.0" and click Install/Update.
The FreeRTOS update for Design Studio must be installed as the following steps:
• Open Window -> Preferences. From the next windows, select S32 Design Studio for S32 Platform -> S32DS Extensions and Updates, click Add All and select the zip archive containing the FreeRTOS update.
• Open Help -> S32DS Extensions and Updates. From the next windows, select "FreeRTOS for S32K3 5.0.0"
then click Install/Update

My S32DS v3.5 + S32K3 RTD 5.0.0 does not encounter this problem.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
894 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Did you follow the chapter 2.2 Installation Design Studio of SW32K3_FreeRTOS_11.1.0_5.0.0_CD1_D2409_ReleaseNotes.pdf?

Make sure S32 Design Studio v3.5.13, S32 Design Studio for S32 Platform v3.5.13 with support for S32K3XXdevices (com.nxp.s32ds.s32k3xx.update_3.5.13.20240726235844.zip, com.nxp.s32ds.s32k396.update_3.5.13.20240726233621.zip and com.nxp.s32ds.update_3.5.13.20240726233529.zip ) and RTD package (SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410_DesignStudio_updatesite.zip ) are installed before this FreeRTOS package.
The S32K3XX RTD update for Design Studio must be installed as the following steps:
• Open Help -> S32DS Extensions and Updates. From the next windows, select "S32K3 Real-Time Drivers AUTOSAR 4.7 R21-11 Version 5.0.0" and click Install/Update.
The FreeRTOS update for Design Studio must be installed as the following steps:
• Open Window -> Preferences. From the next windows, select S32 Design Studio for S32 Platform -> S32DS Extensions and Updates, click Add All and select the zip archive containing the FreeRTOS update.
• Open Help -> S32DS Extensions and Updates. From the next windows, select "FreeRTOS for S32K3 5.0.0"
then click Install/Update

My S32DS v3.5 + S32K3 RTD 5.0.0 does not encounter this problem.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
723 Views
DiaDev
Contributor III

S32DS platform 3.5.14

I have installed the RTD and FreeRTOS packages in DS. I have attached a screenshot showing the installed packages. However, I still get an error during the build process, which I’ve also attached in the screenshot.

0 Kudos
Reply
710 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Why you install S32K3 RTD 3.0.0 with SW32K3 FreeRTOS 11.1.0 version 5.0.0 Code Drop?

FreeRTOS 5.0.0 S32K3 RTD 5.0.0.png

Please install S32K3 RTD 5.0.0 by refer to: HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5
1. Install S32Design Studio 3.5: S32DS.3.5_b220726_win32.x86_64.exe
2. Install Update 13 for S32DS: SW32_S32DS_3.5.13_D2407.zip
3. Install development package for S32K3XX: SW32K3_S32DS_3.5.13_D2407
4. Install development package for S32K396: SW32K39x_S32DS_3.5.13_D2407.zip
5. Install development package for S32M276: SW32M2_S32DS_3.5.13_D2407
6. Install updatesite for this release: SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410_DesignStudio_updatesite.
zip
7. Install SW32K3_FreeRTOS_11.1.0_5.0.0_CD1_D2409_DesignStudio_updatesite.zip