Connection from "127.0.0.1" via 127.0.0.1. Connection from port "51480" to 6224
Connection from "127.0.0.1" via 127.0.0.1. Connection from port "51482" to 7224
PE-ERROR: Warning. Can't read registers while part is running.
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read registers while part is running.
Telnet server running on 127.0.0.1:51794
Searching for Kernel Symbols...
rsp_qC - qSymbol: 5F74785F7468726561645F63757272656E745F707472
_tx_thread_current_ptr not found. ThreadX analysis not enabled.
rsp_qC - qSymbol: 707843757272656E74544342
pxCurrentTCB not found. FreeRTOS analysis not enabled.
PE-ERROR: Warning. Can't read memory while part is running. @4074f0 (2 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @402db0 (2 bytes)
PE-ERROR: Warning. Can't Write Binary while part is running. 0 - Length of: 0 - Value of: Binary Data
PE-ERROR: Warning. Can't Write Binary while part is running. 0 - Length of: 3b8 - Value of: Binary Data
Unable to load libusb0.dll
Copyright 2024 P&E Microcomputer Systems,Inc.
Command Line :C:\NXP\S32DS.3.6.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.9.5.202412131551\win32\pegdbserver_console -device=NXP_S32K3xx_S32K344 -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=5000 -port�
PEmicro Interface detected - Flash Version 11.37
CMD>RE
Initializing.
INFO: DAP IDCODE = 0x6BA02477
INFO: DAP successfully powered up. DP CTRL/STAT = 0xF0000000
Target has been RESET and is active.
CMD>CM C:\NXP\S32DS.3.6.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.9.5.202412131551\supportFiles_ARM\NXP\S32K3xx\nxp_s32k344_1x32x1012k_hse_disabled.arp
Initializing.
INFO: DAP IDCODE = 0x6BA02477
INFO: DAP successfully powered up. DP CTRL/STAT = 0xF0000000
Initialized.
;version 1.03, 11/05/2024, Copyright 2024 P&E Microcomputer Systems, www.pemicro.com [S32K3x4_hse_disabled]
;device nxp, s32k344, 1x32x1012k,desc=hse_disabled
;begin_cs device=$00400000, length=$003F4000, ram=$20400000
Loading programming algorithm ...
Error loading .ARP file : C:\NXP\S32DS.3.6.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.9.5.202412131551\supportFiles_ARM\NXP\S32K3xx\nxp_s32k344_1x32x1012k_hse_disabled.arp at address 20400002
Error loading programming algorithm - load aborted.
Error occured during Flash programming.
INFO: DAP IDCODE = 0x6BA02477
INFO: DAP successfully powered up. DP CTRL/STAT = 0xF0000000
Starting reset script (C:\NXP\S32DS.3.6.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.9.5.202412131551\supportFiles_ARM\NXP\S32K3xx\S32K344.mac) ...
REM Enable clocks for selected cores in MC_ME module
Delaying for 200mS ...
Done.
REM Initialize RAM and DMA:
REM Initialize DMA TCD:
REM Copy valid executable code to RAM for each core to be used.
REM Enable required cores in MC_ME:
Delaying for 20mS ...
Done.
Reset script (C:\NXP\S32DS.3.6.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.9.5.202412131551\supportFiles_ARM\NXP\S32K3xx\S32K344.mac) completed.
PEmicro GDB Launch Failure : Error during flash programming. Terminating debug session.
PE-ERROR: Error downloading to the device. Terminating debug session.
INFO: DAP IDCODE = 0x6BA02477
INFO: DAP successfully powered up. DP CTRL/STAT = 0xF0000000
PE-ERROR: Warning. Can't read memory while part is running. @408a00 (64 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @408afe (2 bytes)
Disconnected from "127.0.0.1" via 127.0.0.1. Disconnection by port "51480" from 6224
Disconnected from "127.0.0.1" via 127.0.0.1. Disconnection by port "51482" from 7224
INFO: DAP IDCODE = 0x6BA02477
Target Disconnected.