S32K344 CAN demo could not send message succeed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K344 CAN demo could not send message succeed

1,013 次查看
KILLERzheng
Contributor IV

I import the CAN demo 'FlexCAN_lp_Example_S32K344' which work mode is loop-back, it works on EVB S32K3X4EVB-Q257 47827 PCB . However, after I changed the work mode from loop-back to 'Normal mode or user mode', and configured the flexCAN0 Rx/Tx, and add the Siul2_Port instance, build it and run, it could not send any message out, even I tried to test the waveform on PT275(on EVB, CAN0 Tx).

Could you please figure out the error place and teach me how to deal with it? Thanks! 

0 项奖励
1 回复

995 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

could below thread be useful for you?

https://community.nxp.com/t5/S32K/S32K344-Evaluation-Board-FlexCan-Example-running/m-p/1343355

There is secure CAN transceiver on the board, TJA1153, which is not configured by default and it does not allow the MCU to communicate with the CAN bus. So a config must be done first.

BR, Petr

0 项奖励