S32K344 CAN communication

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 CAN communication

469 Views
Voledi
Contributor II

Hi NXP team,

I am trying to change FlexCAN_Ip_Example_S32K344 (in loopback mode) to work in normal mode.

In this case I do not care about Transceivers, only care about configuring CAN0_Tx, CAN0_Rx pins to work properly by connecting CAN0_Tx pin to Logic Analyzer, and also connecting CAN0_Tx and CAN0_Rx together---> The result is that I do not see any digital signal from Tx pin to Logic Analyzer, and Rxbuffer is also empty:
below is my change:

Voledi_0-1735194405041.png

Voledi_1-1735194446487.pngVoledi_2-1735194484267.png

 

please give me help, thanks

0 Kudos
Reply
1 Reply

435 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Voledi

It's Christmas holiday recently, so the reply is a bit slow.
You can try adding the following pins, and then directly measure the PTA7 pin of MCU

Senlent_0-1735287074548.png

 

0 Kudos
Reply