S32K344 ADC Use of external channels

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344 ADC Use of external channels

1,180件の閲覧回数
Albatros
Contributor III

I understood how to use external channels in S32K344 but want to learn how will it benefit me to use them?

タグ(3)
0 件の賞賛
返信
1 返信

1,133件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

Each ADC provides 3 external decode signals (MA) to be used to select one channel, out of a maximun of 8, from external analog multiplexers. And there can be maximum 4 of such multiplexers to connect 32 external channels, it means that these 4 multiplexers sharing the same MA signals.

The ADC automatically sets the MA to control these external analog multiplexers, based on the current channel selected for conversion. Depending on the Mask Register bits, the corresponding “X” pin is sampled, and the result is stored in the matching location for the “MA” & “X” combination.

Hope it helps you. 

Have a nice day!

0 件の賞賛
返信