S32K344 搭配DP83848YB/NOPB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 搭配DP83848YB/NOPB

2,056 Views
wangjunxiao
Contributor I

请问有没有k344搭配DP83848YB/NOPB实现的demo?

0 Kudos
Reply
11 Replies

2,035 Views
wangjunxiao
Contributor I

我安装的RTD版本是SW32K3_RTD_4_4_2_0_0_D2203,我没有找到对应这个版本的TCP/IP STACK包,请问在不升级RTD版本的情况下要怎么做?

0 Kudos
Reply

2,029 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@wangjunxiao

我尝试安装了下STACK,在旧版是上有点问题,目前我是可以在RTD 2.0.1运行stack。如果你的工程目前只能使用RTD 2.0.0,那我建议你安装完RTD 2.0.1之后,配置为stack,再将配置文件移植到RTD 2.0.0版本上。lwip_s32k344这个demo是基于RTOS,没有发现还有别的demo提供。

0 Kudos
Reply

1,998 Views
wangjunxiao
Contributor I

我在文档里看到这个建议,请问VDD_HV_B的电压必须要提高到5V吗?我们的是3.3V,对网口调试会有什么影响吗?20230617-192730.jpg

0 Kudos
Reply

1,815 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@wangjunxiao

没测试过,但是看到类似的回答如下:

You will have to move the jumper J30 on eval board from position 3-4 CLOSED to 1-2 CLOSED in order for on-board Ethernet level shifters to work properly.

0 Kudos
Reply

1,804 Views
wangjunxiao
Contributor I

我已参考配LEIP_S32K344 DEMO GUIDE 文档置了相关信息,在调试中遇到了这个问题,一直在while循环里,等待建立连接,请问出现这个问题的原因可能在哪里?

20230617-192542.jpg

0 Kudos
Reply

1,799 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@wangjunxiao

我没有硬件,没测试过这个demo,不熟悉改方案。

请用英文将你的问题描述清楚,会有熟悉这个方案的工程师帮你解答。

下次,如果有新的问题就创建一个新的topic。

0 Kudos
Reply

1,795 Views
wangjunxiao
Contributor I
好的感谢
0 Kudos
Reply

2,000 Views
wangjunxiao
Contributor I

我已参考配LEIP_S32K344 DEMO GUIDE 文档置了相关信息,在调试中遇到了这个问题,一直在while循环里,等待建立连接,请问出现这个问题的原因在哪里?20230617-192542.jpg

0 Kudos
Reply

2,023 Views
wangjunxiao
Contributor I

好的,谢谢~

0 Kudos
Reply

2,049 Views
Senlent
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,043 Views
wangjunxiao
Contributor I

 This TCP/IP stack release is intended to be used as integrated with S32 RTD drivers and FreeRTOS in a non-AUTOSAR based environment.

请问不跑嵌入式操作系统的demo有吗?example里只有回环测试

0 Kudos
Reply