S32K344电源上下电时序要求

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344电源上下电时序要求

128 Views
liyongfeng
Contributor II

请问S32K3对V15与VDD_HV_A(B)之间给电/断电的时序有什么要求吗?如果违反会造成什么故障现象?

0 Kudos
Reply
1 Reply

109 Views
PavelL
NXP Employee
NXP Employee

Hi,

There is no power sequence required for the S32K3. Rather an MCU Power Supply Ramp rate consideration. From the S32K3 hardware design guidelines:

2.10.1 MCU Power Supply Ramp rate
In the S32K3XX datasheet, there is a parameter called "MCU supply ramp rate" with a maximum and a minimum limit. During the power-on of MCU, the power supply must assure a ramp-rate within this range from VDD_OFF=0.1V to the voltage operating level of VDD_HV_A, VDD_HV_B and V15. The outcome of violating the specification causes unexpected behavior, stuck operation or damage in the MCU.

Best Regards,

Pavel

0 Kudos
Reply