S32K342 LPUART unexpected signal interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K342 LPUART unexpected signal interrupt

跳至解决方案
1,910 次查看
towenyu
Contributor III

To simpify issues I encountered with S32K342 development, I started new project from standard example: 

S32K3 RTD AUTOSAR 4.42.0.0 D2203 Example Projects -> Pit_Ip_example_S32K342

After successfully compiled and run, I added module LPUART to this project and assigned two ports for LPUART3:

towenyu_0-1709706434818.png

 

And pretty default setting for LPUART module except change baudrate to 115200:

towenyu_1-1709706746669.png

 

Then program always get hang at a Uart_Send_Data_int() function:

towenyu_2-1709706901110.png

code for this function is pretty simple:

towenyu_3-1709707011146.png

 

No idea of what could possiblly wrong. Only two interrupt enabled:  PIT0 and LPUART3. Still wrong after diabled PIT0. 

For comparison I created another example:  LpuartFlexio_Uart_Ip_Example_S32K342.  Using previous function and everything runs well.

Is there any similiar story anyone encounted? Highly appreciate letting me know what's went wrong.

 

Thanks and Best Regards,

Yu Wen

0 项奖励
回复
1 解答
1,887 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Yu Wen,

You need to define the interrupt hander:

LPUART_UART_IP_3_IRQHandler

danielmartynek_0-1709818075566.png

 

Regards,

Daniel

 

 

在原帖中查看解决方案

5 回复数
1,905 次查看
towenyu
Contributor III

BTW I also checked memory map against linker file, looks like at least it fits in memory range. But I'm not so sure about it, so it would be great if anyone could help check those two files.

0 项奖励
回复
1,897 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @towenyu,

Can you please attach the whole project?

 

Thanks,

BR, Daniel

标记 (1)
1,891 次查看
towenyu
Contributor III

Here is the whole project. And this can be pretty easily reproduced by starting from example project and add LPUART module...

Thanks for helping,

Best Regards,

Yu Wen

0 项奖励
回复
1,888 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Yu Wen,

You need to define the interrupt hander:

LPUART_UART_IP_3_IRQHandler

danielmartynek_0-1709818075566.png

 

Regards,

Daniel

 

 

1,877 次查看
towenyu
Contributor III

Thanks and your suggestion solved my issue.

 

Strange though I didn't manually input handler name, I guess it is automatically filled; somehow this time the tool didn't do that for me. 

Maybe it is worthy to check the consistance -- as it has been check and enabled in "interrupt controller" page.

Thanks and Best Regards,

Yu Wen

0 项奖励
回复