S32K341 Crystal oscillator power is not applied.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K341 Crystal oscillator power is not applied.

Jump to solution
2,307 Views
Masaki_Mori
Contributor II

I finished checking the operation using S32K3X4EVB and made a per_pin board for S32K341. I wrote the S32K3X4EVB firmware, but power is not applied to the crystal oscillator circuit.

0 Kudos
Reply
1 Solution
2,227 Views
Masaki_Mori
Contributor II

Hi, Daniel

I made a mistake in attaching the emitter and base of the transistor. This problem is resolved. Thanks.

View solution in original post

4 Replies
2,282 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Masaki_Mori,

Can you share the schematic? If not here, please create a ticket.

Have you checked the power supply?

Can you load the project to the S32K341 MCU on that board?

 

Best regards,

Daniel

0 Kudos
Reply
2,265 Views
Masaki_Mori
Contributor II

I have not created the schematic. Application of power has already been confirmed. It seems that the project is being written to the S32K341 . A 256Hz self-oscillation output can be seen at the MCU reset terminal PTA05.

0 Kudos
Reply
2,247 Views
danielmartynek
NXP TechSupport
NXP TechSupport

HI @Masaki_Mori,

Can you disable Run on reset in the debug configuration and step through the code from the reset vector after the image has been loaded? Is there is Fault exception detected?

danielmartynek_0-1708339239997.png

 

Regards,

Daniel

 

0 Kudos
Reply
2,228 Views
Masaki_Mori
Contributor II

Hi, Daniel

I made a mistake in attaching the emitter and base of the transistor. This problem is resolved. Thanks.