Hi, experts
we are working on S32K324, and use pwm trigger ADC interrupt for every 28us in core1, inside ADC interrupt, we put some control logic code, but we found that the ADC interrupt execution time is near 24us(including ADC function plus our control logic), we measure the time via toggle pin, so this issue will cause OS task delay. now we are using RTD SW32K3_S32M27x_RTD_R21-11_5.0.0.
In our last project, we didn't implement autosar os in core1, and use SW32K3_RTD_4.4_2.0.0, the ADC interrupt execution time is only 12us.
so what can we do to reduce ADC interrupt execution time?
Hi@witness248
From your phenomenon, it seems that the clock distribution settings are different.
Have you checked whether the ADC clock settings are the same?
etc,"Core clock" and "Adc Prescaler Value".
Are the sampling parameter settings consistent, that is "Adc Unit Normal Sampling Duration x"?
hi, Senlent
Thanks for your reply. for ADC module clock, it is correct. and now we are planning to put the ADC ISR function into ITCM area, but I don't know how to do it, could give me some tutorial?
1. if I put itcm_text at the beginning of the SECTIONS, like below:
it can compile pass, but no data at 0x00000000
2. If I put itcm_text at the below location:
some compile errors happen.
Hi@witness248
Here is a demo in our knowledgebase, you can refer to it.
There are many versions of RTD. The link files and startup files of each version may be different, but the principles are exactly the same. You must initialize before accessing