Hi
S32K324也是下载S32K344的HSE FW和SBAF.
S32K3 Standard Software -> Automotive SW - S32K3 - Secure BAF (SBAF)
S32K3 Standard Software -> Automotive SW - S32K3 - HSE Firmware
目前最新的版本是:
0.15.0 S32K344 SBAF 0.15.0 RTM Release
0.2.40.0 S32K344 HSE FW 0.2.40.0 SR Release
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi
S32K324也是下载S32K344的HSE FW和SBAF.
S32K3 Standard Software -> Automotive SW - S32K3 - Secure BAF (SBAF)
S32K3 Standard Software -> Automotive SW - S32K3 - HSE Firmware
目前最新的版本是:
0.15.0 S32K344 SBAF 0.15.0 RTM Release
0.2.40.0 S32K344 HSE FW 0.2.40.0 SR Release
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
hi,
非常感谢你的回答,我还有2个问题想咨询下:
1.SBAF是出厂自带的,那么S32K324芯片出厂自带的SBAF版本号是多少呢?如果我直接使用0.2.40.0版本的HSE固件会造成和出厂SBAF版本不兼容吗?
2.如果我将SBAF版本更新到0.0.15.0版本,那么0.0.40.0的HSE固件版本会和0.0.15.0版本的SBAF不兼容吗?
Best Regards,
Wiho
1. SBAF出厂自带的,根据出厂日期不同默认的SBAF版本不同。你也可以通过0x4039C020查看SBAF版本号。请看RM758223-HSE-B Firmware Reference Manual - V2.3(2.3).pdf的 Table 140. Secure BAF version number HSE GPR (0x4039C020)。 至于SBAF和HSE FW版本兼容性,请看RM758223-HSE-B Firmware Reference Manual - V2.3(2.3).pdf的14.7 HSE Firmware and Secure BAF release version compatibility章节。
2. SBAF版本0.0.15.0和HSE FW版本0.2.40.0是兼容的。
您好,我想问一下如果HSE firmware一直就固定在一个版本上,但是SBAF随着芯片出厂日期一直更新最新版本的话,会不会有可能出现SBAF和一直固定的这个HSE firmware不兼容的情况出现?