S32K314 secure boot: BSB mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K314 secure boot: BSB mode

Jump to solution
2,272 Views
liTian_one
Contributor II

After program the relevant firmware for enabling secure boot, and after powering off and on again, the software remained at 0x2040012e.

What could be the reason for this?  Or is there any way I can find out the cause?

liTian_one_1-1756637375754.png

 

 

0 Kudos
Reply
1 Solution
2,131 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

How did you generated the GMAC? Do you follow the S32K344_Basic_SecureBoot example or do you generate the GMAC externally? Maybe this could be useful for you:

https://community.nxp.com/t5/S32K/Request-for-PC-side-GMAC-example-for-S32K344-Basic-Secure-Boot/td-...

View solution in original post

0 Kudos
Reply
4 Replies
2,163 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @liTian_one 

The device is in recovery mode. This mode is entered when: IVT is not present or corrupted or there are more than 8 consecutive functional/destructive resets or when secure boot fails.

In case of JTAG recovery mode, the device just hangs in endless loop in RAM, so user can take appropriate actions and the device is not bricked.

Based on your description, it’s caused by failing secure boot.

 

You can follow demo code from:

https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples

Example:

c:\NXP\S32K3_HSE_DemoExamples_1_0_0\S32K3_HSE_DemoExamples\Secure_Boot\S32K344_Basic_SecureBoot\

 

We also provide Secure Boot application note including demo projects. It can be downloaded from:

https://www.nxp.com/products/S32K3

Application note can be found here:

Documentation -> Secure Files -> Secure Boot Application note v0.1.1.0 (AN744511)

Associated demo project can be downloaded here:

Design Resources -> Software -> Secure Files -> SecureBootAppNoteDemo (SW745310)

 

Common problem is wrong alignment of your application. Please take a look at this section from the application note:

lukaszadrapa_0-1756708389147.png

 

Regards,

Lukas

0 Kudos
Reply
2,160 Views
liTian_one
Contributor II
The settings of IVT (0x00400000) should be correct, and the addresses of APP header and APP code are (0x004020c0) and (0x00402100) respectively.
0 Kudos
Reply
2,132 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

How did you generated the GMAC? Do you follow the S32K344_Basic_SecureBoot example or do you generate the GMAC externally? Maybe this could be useful for you:

https://community.nxp.com/t5/S32K/Request-for-PC-side-GMAC-example-for-S32K344-Basic-Secure-Boot/td-...

0 Kudos
Reply
2,117 Views
liTian_one
Contributor II
The cause of the problem has been identified.thank you
0 Kudos
Reply