S32K314:cann`t wakeup from standby

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K314:cann`t wakeup from standby

779 次查看
Jingjing
Contributor I

hello:

I encouter a problem that:after called Power_Ip_SetMode(SOC_STANDBY),the current is 0.01A,when use gpio to wakeup,the board cann`t wakeup from standby.

i want ask that:

1. how to confirm  the board enter to standby success?

2. all clock disable or other?if also have ips active when standby,the board cann`t enter standby entirely?   

3. how to set the board entirely enter to standby? can give me a example to see?

thank you very much.

0 项奖励
4 回复数

759 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Jingjing 

Please refer Table 25. STANDBY of the RM, this table in the section 4.5.8 mentions the state of pins of the device under standby mode.
Also take a look at this community post, where are attached some examples that can be helpful for you.
Wakeup MCU from standby 

 

B.R

VaneB

0 项奖励

740 次查看
Jingjing
Contributor I

thank you for reply.

"Please refer Table 25. STANDBY of the RM, this table in the section 4.5.8 mentions the state of pins of the device under standby mode."

which document mention the " the state of pins of the device under standby mode" ?

0 项奖励

726 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Jingjing 

The document is the reference manual, you can dowload at the following link: 

S32K3XXRM 

0 项奖励

720 次查看
Jingjing
Contributor I

I get it ,thank you.

标记 (1)
0 项奖励