S32K314:cann`t wakeup from standby

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K314:cann`t wakeup from standby

786 Views
Jingjing
Contributor I

hello:

I encouter a problem that:after called Power_Ip_SetMode(SOC_STANDBY),the current is 0.01A,when use gpio to wakeup,the board cann`t wakeup from standby.

i want ask that:

1. how to confirm  the board enter to standby success?

2. all clock disable or other?if also have ips active when standby,the board cann`t enter standby entirely?   

3. how to set the board entirely enter to standby? can give me a example to see?

thank you very much.

0 Kudos
4 Replies

766 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Jingjing 

Please refer Table 25. STANDBY of the RM, this table in the section 4.5.8 mentions the state of pins of the device under standby mode.
Also take a look at this community post, where are attached some examples that can be helpful for you.
Wakeup MCU from standby 

 

B.R

VaneB

0 Kudos

747 Views
Jingjing
Contributor I

thank you for reply.

"Please refer Table 25. STANDBY of the RM, this table in the section 4.5.8 mentions the state of pins of the device under standby mode."

which document mention the " the state of pins of the device under standby mode" ?

0 Kudos

733 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Jingjing 

The document is the reference manual, you can dowload at the following link: 

S32K3XXRM 

0 Kudos

727 Views
Jingjing
Contributor I

I get it ,thank you.

Tags (1)
0 Kudos