S32K312EVB-Q172 <> FRDM665SPIEVB : Can we stack S32K312 eval board and M665S eval board ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312EVB-Q172 <> FRDM665SPIEVB : Can we stack S32K312 eval board and M665S eval board ?

119 Views
varunbharti
Contributor II

hi, 

Can we stack the FRDM665SPIEVB eval board directly on top of the S32K312EVB-Q172 eval board?

Also, if it is possible to stack, can the S32K312EVB-Q172 be powered from FRDM665SPIEVB pins directly?

I appreciate any help you can provide.

0 Kudos
Reply
1 Reply

103 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

UM11734 Hardware user manual for FRDM665SPIEVB.pdf only mentions: Connectors to interface directly with S32K344EVB-Q172 launchpad.   No mention of S32K312EVB-Q172.
I am afraid you need to open the schematics of S32K344EVB-Q172 and S32K312EVB-Q172 and compare the pinouts of ARDUINO Headers to see if they are consistent. Pay attention to the signals mentioned in Tab. 10 - Tab. 15 for S32K344EVB connector - K1 to K6 of UM11734.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------