S32K312 flexio i2c consecutive channel pairings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 flexio i2c consecutive channel pairings

245 Views
sf_en
Contributor II

sf_en_0-1748912965727.png

 I am using two pins as show above as flexio i2c,

when configure in EB, below errors occur.

I2c hardware channel used is FLEXIO_0_CH_2_3. For SDA Channel Ref select CHANNEL_3 of the FLEXIO device

I2c hardware channel used is FLEXIO_0_CH_2_3. For SCL Channel Ref select CHANNEL_2 of the FLEXIO device.

In hardware design, acturally using CHANNEL_3 as SCL and CHANNEL_2 as SDA.

Is there restictions that "The SCL channel must always be the lower-numbered channel in the pair" in S32K312?

Tags (1)
0 Kudos
Reply
1 Reply

213 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please swap the pins in Flexio_I2c or Flexio_Mcl_Ip.

Flexio_I2c SCL SDA Channel Ref.pngFlexio_Mcl_Ip Flexio Logic Channel.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply