S32K312 eval board power consumption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K312 eval board power consumption

ソリューションへジャンプ
1,151件の閲覧回数
buccno
Contributor III

Hello, I'm working on an eval board with an S32K312, and I'm investigating the RUN and STANDBY modes. When I input the peripherals active in the RUN mode into the S32K Power Estimation Tool, I see that the board draws almost the same current.

buccno_0-1700847765860.png

However, when it goes into standby mode, instead of 660uA, I see 23mA. What could be the reason for this?

I am not able to measure the current from the pins; I am observing it from the power supply. The power supplied to the board is 12V. (I use FXOSC for standby btw)

0 件の賞賛
返信
1 解決策
1,130件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @buccno 

this measures the current consumption of whole board, not just consumption of the MCU. It's not so significant in run modes but but it's definitely not usable for low power modes.

Take a look at jumper J10. This is copied from schematic and user manual:

https://www.nxp.com/webapp/Download?colCode=S32K312EVBQ172_CAD_FILES_REVA1

lukaszadrapa_0-1701103220976.png

lukaszadrapa_1-1701103226248.png

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,131件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @buccno 

this measures the current consumption of whole board, not just consumption of the MCU. It's not so significant in run modes but but it's definitely not usable for low power modes.

Take a look at jumper J10. This is copied from schematic and user manual:

https://www.nxp.com/webapp/Download?colCode=S32K312EVBQ172_CAD_FILES_REVA1

lukaszadrapa_0-1701103220976.png

lukaszadrapa_1-1701103226248.png

Regards,

Lukas

0 件の賞賛
返信