S32K312 eval board power consumption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 eval board power consumption

Jump to solution
1,167 Views
buccno
Contributor III

Hello, I'm working on an eval board with an S32K312, and I'm investigating the RUN and STANDBY modes. When I input the peripherals active in the RUN mode into the S32K Power Estimation Tool, I see that the board draws almost the same current.

buccno_0-1700847765860.png

However, when it goes into standby mode, instead of 660uA, I see 23mA. What could be the reason for this?

I am not able to measure the current from the pins; I am observing it from the power supply. The power supplied to the board is 12V. (I use FXOSC for standby btw)

0 Kudos
Reply
1 Solution
1,146 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @buccno 

this measures the current consumption of whole board, not just consumption of the MCU. It's not so significant in run modes but but it's definitely not usable for low power modes.

Take a look at jumper J10. This is copied from schematic and user manual:

https://www.nxp.com/webapp/Download?colCode=S32K312EVBQ172_CAD_FILES_REVA1

lukaszadrapa_0-1701103220976.png

lukaszadrapa_1-1701103226248.png

Regards,

Lukas

View solution in original post

0 Kudos
Reply
1 Reply
1,147 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @buccno 

this measures the current consumption of whole board, not just consumption of the MCU. It's not so significant in run modes but but it's definitely not usable for low power modes.

Take a look at jumper J10. This is copied from schematic and user manual:

https://www.nxp.com/webapp/Download?colCode=S32K312EVBQ172_CAD_FILES_REVA1

lukaszadrapa_0-1701103220976.png

lukaszadrapa_1-1701103226248.png

Regards,

Lukas

0 Kudos
Reply