S32K312 OpenSDA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 OpenSDA

Jump to solution
3,104 Views
AnhNguyenDuc
NXP Employee
NXP Employee

Hello everyone, I have a question about S32K312.

Which UART, S32K312's OpenSDA used ? And what pins.

Thank you.

0 Kudos
Reply
1 Solution
3,030 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please download through the link I sent you privately.

View solution in original post

0 Kudos
Reply
5 Replies
3,023 Views
Dr_Bubo
Contributor I

Hi Robin,

we have also started development with K312 therefore I would have interested on this link as well. Could you send it me too? 

0 Kudos
Reply
3,001 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Bubo,

This file is not currently publicly available and you are advised to contact a sales representative. LoveEmbedded181 is colleague, so I sent him a link that can only be downloaded from the intranet.

Best Regards,
Robin

0 Kudos
Reply
3,072 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi LoveEmbedded181,

Please download the S32K312EVB-Q172_HW_PackRevA1.zip and then you can find the information in S32K312EVB-Q172_PackRevA1_HardwareUserManual.pdf.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
3,050 Views
AnhNguyenDuc
NXP Employee
NXP Employee

Hi Robin_Shen,

Can you give me a link to get .zip file

Tags (1)
0 Kudos
Reply
3,031 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please download through the link I sent you privately.

0 Kudos
Reply