S32K312 EVK power issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K312 EVK power issue

1,550 次查看
ajnas-c
Contributor I

Hi,

We are using a S32k312 EVK for our development, Today suddenly the device is not responding when we are powered up the device. We are checked the all the voltages in the board, only the input supply is coming the PMIC(FS26) outputs are LOW (0V). The PMIC input is coming properly but the outputs not.

Any solution?

0 项奖励
回复
4 回复数

1,534 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Before stating that the EVK was damaged, could you provide us the resistance between TP51 and GND? Should not be close to 0.

If the resistance is close to 0, could be that a capacitor was shorted hence causing the 0 V on the output.

Please, let us know.

0 项奖励
回复

1,529 次查看
ajnas-c
Contributor I
Hi,
We are getting 22k between TP51 and GND.
0 项奖励
回复

1,499 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Using an Oscilloscope, can you measure the following signal:

- VPRE_SW

Could you provide the memory read-out of your PMIC? To see what is flashed on the part.

Please, let us know.

 

0 项奖励
回复

1,546 次查看
ajnas-c
Contributor I

This is the readings we are getting

image.png

0 项奖励
回复