Hello
I set PTC2 to CAN RX mode in pin init config.
Can I change PTC2 to EIRQ[2] during runtime ?
Without change pin init config.
And also, back to CAN RX mode during runtime ?
Thank you
const Siul2_Port_Ip_PinSettingsConfig g_pin_mux_InitConfigArr0[NUM_OF_CONFIGURED_PINS0] =
{
{
.base = IP_SIUL2,
.pinPortIdx = 66u,
.mux = PORT_MUX_AS_GPIO,
.safeMode = PORT_SAFE_MODE_DISABLED,
.inputFilter = PORT_INPUT_FILTER_DISABLED,
.driveStrength = PORT_DRIVE_STRENTGTH_DISABLED,
.pullConfig = PORT_INTERNAL_PULL_NOT_ENABLED,
.slewRateCtrlSel = PORT_SLEW_RATE_SLOWEST,
.pullKeep = PORT_PULL_KEEP_DISABLED,
.invert = PORT_INVERT_DISABLED,
.inputBuffer = PORT_INPUT_BUFFER_ENABLED,
.outputBuffer = PORT_OUTPUT_BUFFER_DISABLED,
.adcInterleaves = { MUX_MODE_NOT_AVAILABLE, MUX_MODE_NOT_AVAILABLE },
.inputMuxReg = {
0u
},
.inputMux = {
PORT_INPUT_MUX_ALT1,
PORT_INPUT_MUX_NO_INIT,
PORT_INPUT_MUX_NO_INIT,
PORT_INPUT_MUX_NO_INIT,
PORT_INPUT_MUX_NO_INIT,
PORT_INPUT_MUX_NO_INIT,
PORT_INPUT_MUX_NO_INIT,
PORT_INPUT_MUX_NO_INIT
},
},
};
已解决! 转到解答。