S32K3 support for IEC 60730 Software Class B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 support for IEC 60730 Software Class B

ソリューションへジャンプ
3,371件の閲覧回数
JasonG
Contributor I

Hi there, 

We'd love to make use of the S32K3 in our next generation of products. Some of our existing customers require the products to be IEC 60730 Software Class B compliant. 

Is it possible to implement the IEC 60730 Software Class B on the S32K3? And is there any existing libraries/modules/support for the IEC 60730B tests on the S32K3. 

If not, any suggestions would be appreciated. 

Kind regards, 
Jason 

0 件の賞賛
返信
1 解決策
3,360件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

S32K3 is automotive device, therefore it is compliant with automotive standards.

The S32K3 MCUs of 32/bit AEC-Q100 qualified MCUs combine a scalable family of Arm® Cortex®-M7-based microcontrollers in single, dual, and lockstep core configurations, supporting up to ASIL D functional safety automotive and industrial applications.

Is it possible to implement the IEC 60730 Software Class B on the S32K3?

I expect that this micro will easily fit any industrial standard as its target is ASIL-D which is most strict automotive one.

And is there any existing libraries/modules/support for the IEC 60730B tests on the S32K3.

No direct support for IEC 60730B is available.

There is SAF (safety application framework) to help customers achive ASIL-D. The micro also has many HW self-test mechanisms in order to achieve safe operation in automotive.

https://www.nxp.com/design/automotive-software-and-tools/s32-safety-software/s32-safety-software-fra...

Best regards,

Pter

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,361件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

S32K3 is automotive device, therefore it is compliant with automotive standards.

The S32K3 MCUs of 32/bit AEC-Q100 qualified MCUs combine a scalable family of Arm® Cortex®-M7-based microcontrollers in single, dual, and lockstep core configurations, supporting up to ASIL D functional safety automotive and industrial applications.

Is it possible to implement the IEC 60730 Software Class B on the S32K3?

I expect that this micro will easily fit any industrial standard as its target is ASIL-D which is most strict automotive one.

And is there any existing libraries/modules/support for the IEC 60730B tests on the S32K3.

No direct support for IEC 60730B is available.

There is SAF (safety application framework) to help customers achive ASIL-D. The micro also has many HW self-test mechanisms in order to achieve safe operation in automotive.

https://www.nxp.com/design/automotive-software-and-tools/s32-safety-software/s32-safety-software-fra...

Best regards,

Pter

 

0 件の賞賛
返信
3,326件の閲覧回数
JasonG
Contributor I
Hi Peter,

Thank you for your response. That is great to hear that there is at least some pathway to support the standard.

Kind regards,
Jason
0 件の賞賛
返信