S32K3 XRDC with PID

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 XRDC with PID

Jump to solution
1,642 Views
oskarjohansson
Contributor I

I am using S32K344 with RTD 2.0.0 D2203 and want to use the RM module in the MCAL to setup different domains for different PID. 

I want to use the PID to filter on the domain assignment for the core, but any option is greyed out and I cannot find an option to enable it. 

oskarjohansson_0-1694753896315.png

Best regards,

Oskar Johansson

 

0 Kudos
Reply
1 Solution
1,605 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @oskarjohansson 

If you expand the Xrdc PID Enable tab, you will be able to see that is disabled. That is the reason the options are greyed out. Once you change the mentioned value, the PID options can be changed. 

VaneB_1-1694803637341.png

 

B.R.

VaneB

View solution in original post

0 Kudos
Reply
1 Reply
1,606 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @oskarjohansson 

If you expand the Xrdc PID Enable tab, you will be able to see that is disabled. That is the reason the options are greyed out. Once you change the mentioned value, the PID options can be changed. 

VaneB_1-1694803637341.png

 

B.R.

VaneB

0 Kudos
Reply