I am using S32K344 with RTD 2.0.0 D2203 and want to use the RM module in the MCAL to setup different domains for different PID.
I want to use the PID to filter on the domain assignment for the core, but any option is greyed out and I cannot find an option to enable it.
Best regards,
Oskar Johansson
Solved! Go to Solution.
If you expand the Xrdc PID Enable tab, you will be able to see that is disabled. That is the reason the options are greyed out. Once you change the mentioned value, the PID options can be changed.
B.R.
VaneB
If you expand the Xrdc PID Enable tab, you will be able to see that is disabled. That is the reason the options are greyed out. Once you change the mentioned value, the PID options can be changed.
B.R.
VaneB