S32K3 - Wake Up Failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 - Wake Up Failed

354 Views
Reyxx
Contributor I

Hi NXP,

         I'm using WKPU mode of S32K314. I config PTE6 port as wake up source with Falling Edge, which has external pull-up on board.

         After MCU enters standby mode,  I connect PTE6 port to a continuous low level. However, there is a very low probability of MCU wake-up failure,1% or less.

        Could you please tell me why?

Best Regards.

 

Tags (3)
0 Kudos
Reply
1 Reply

323 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Reyxx,

I don't think this is related to the WKPU module or the MCU. Since this is less than 1% of cases, it is really hard to pinpoint. Could you share the steps to measure this result of 1%? Are you constantly going to standby and waking up, measuring the current?

If possible, please share the configuration used for going to standby. 

Also, please try to test this using an evaluation board and see if the same number of times the wake up fails. This could be erroneous triggering by glitches in HW as well.

Best regards,
Julián

0 Kudos
Reply