S32K3 Unified Bootloader Build Issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K3 Unified Bootloader Build Issue

跳至解决方案
5,593 次查看
YL005
Contributor III

Hi,

I want to try the unified bootloader V2.1 with my S32K344 EVB, but I can't compile the project successfully.

Can anyone tell me which RTD I should use or what the configuration of the environment can build the project without error.

For now, my configuration are listed below:

  • S32DS for S32 Platform 3.4
  • S32K3 RTD AUTOSAR 4.4 Version 2.0.0

The error message:

error messages.png

The following link is the project I used.

Unified bootloader Demo - NXP Community

 

Thanks

0 项奖励
回复
1 解答
5,541 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

1. Offline install SW32K3_S32DS_3.4.3_D2112.zip

SW32K3_S32DS_3.4.3_D2112.pngSW32K3_S32DS_3.4.3_D2112 installed.png

2. Install SW32K3 RTD 4.4 2.0.0

install S32K3 RTD2.0.0.pngS32K3 RTD2.0.0 installed.png

3. Extract to S32K344_CAN_Bootloader_RTD2d0

Extract to S32K344_CAN_Bootloader_RTD2d0.png

4. Import S32K344_CAN_bootlloader_RTD2d0

Import S32K344_CAN_bootlloader_RTD2d0.png

5. Build Debug_FLASH

Build Debug_FLASH S32K344_CAN_bootlloader_RTD2d0.png

在原帖中查看解决方案

8 回复数
2,734 次查看
ShishirShah
Contributor I

I can not find SW32K3_S32DS_3.4.3_D2112.zip anymore in the NXP repository. Can somebody provide a link or the file itself please? Thank you in advance !

0 项奖励
回复
2,722 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry, this is an old software package, so you may not have access to it. Have you tried to online install the dependencies software packages via S32DS Extensions and Updates?

0 项奖励
回复
4,481 次查看
JonAnder_Amante
Contributor II

Hi, I am using the project "S32K344_Can_bootloader_RTD200" in the microprocessor S32K344. I want to download an application with the program of bootloader. I have achieved the jump from program to application but I have different questions. 1. I want to use #define EN_DELAY_TIME but when I uncomment the command in the folder "public_in", the program has different errors. My target to use "Backdoor", that is to say, I want to check if the program has to enter to bootloader or not. I don´t know the process and the different functions that I have to use to achieve the target. I want to use the function "Boot_CheckReqBootloaderMode(void)" but when I debug the program, it never enters to the "if". Could you explain me the process and the steps to achieve the target. I add different functions that I think are important. 2. I don´t know if I have to modificate the parameters of "static tJumpAppDelayTimeInfo gs_stJumpAPPDelayTimeInfo = {FALSE, 0u};". I have to change this structure ? You can see all structure in one of the next pictures. I need the reply as soon as possible since I have to send a project very soon. 

 

JonAnder_Amante_0-1713767579062.png

 

 

 

 

 

JonAnder_Amante_1-1713767579064.png

 

 

 

 

 

JonAnder_Amante_2-1713767579066.png

 

 

 

 

 

JonAnder_Amante_3-1713767579068.png

 

 

 

 

 

JonAnder_Amante_4-1713767579067.png

 

 

Thank you for all,

0 项奖励
回复
5,567 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

My S32DS v3.4 already installed S32K3 RTD AUTOSAR 4.4 version 2.0.0 and 2.0.1 and 2.0.3 . If I import the S32K344_APP_Demo_RTD2d0 and S32K344_CAN_Bootloader_RTD2d0 projects and build directly, there will be no error. But because a newer version of RTD is installed, an error will be reported if I click Update Codes and then build again.

The project in unified_bootloader_demo_v2.1 appears to be based on S32K3 RTD AUTOSAR 4.4 version 2.0.0.
Please try Offline Package Installation Setup:
SW32K3_S32DS_3.4.3_D2112.zip  SW32K3_S32DS_3.4.3_D2205.zip
SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204.zip

Automotive SW - S32K3 Standard Software.pngAutomotive SW - S32K3 - S32 Design Studio 3.4.3_D2112.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励
回复
5,557 次查看
YL005
Contributor III

Thank you for the quick reply.

I try to install the the version you mentioned.

InstalledVersion.png

But still error messages here

YL005_0-1684473377334.png

Is there anything I can do to deal with these errors?

0 项奖励
回复
5,542 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

1. Offline install SW32K3_S32DS_3.4.3_D2112.zip

SW32K3_S32DS_3.4.3_D2112.pngSW32K3_S32DS_3.4.3_D2112 installed.png

2. Install SW32K3 RTD 4.4 2.0.0

install S32K3 RTD2.0.0.pngS32K3 RTD2.0.0 installed.png

3. Extract to S32K344_CAN_Bootloader_RTD2d0

Extract to S32K344_CAN_Bootloader_RTD2d0.png

4. Import S32K344_CAN_bootlloader_RTD2d0

Import S32K344_CAN_bootlloader_RTD2d0.png

5. Build Debug_FLASH

Build Debug_FLASH S32K344_CAN_bootlloader_RTD2d0.png

3,399 次查看
Sukumar21
Contributor III

How did you got it build without C40_Ip_StartSequenceInit error? I am doing the same as mentioned in this post but getting error

标记 (1)
0 项奖励
回复
5,500 次查看
YL005
Contributor III

Hi @Robin_Shen 

The step by step instructions are helpful, I can build the project successfully now.

I finally figured out that if I import the project without copying it to the workspace, I get an error when building the project. On the contrary, if I choose to copy project into the workspace while importing the project, then the project will build successfully.

I'm not sure why this happened, but at least the project can build now.

Thank you so much.

YL005_0-1684736875758.png

YL005_1-1684736977066.png

 

 

0 项奖励
回复