S32K3 Secure Boot used ASB mode,but it only work well only once

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 Secure Boot used ASB mode,but it only work well only once

436 Views
rujunzhou
Contributor III

Hello:

    After installing Secure Boot, I took measures to reset it. Then flash the file into the MCU, and when powered on for the first time, it can jump to APPBL normally. I will use CAN to send messages in APPBL. After powering off again, the CAN message cannot be received, and the entire controller is powered off. Document image 111/1000 real-time translation After installing Secure Boot, I took measures to reset it. Then flash the file into the MCU, and when powered on for the first time, it can jump to APPBL normally. I will use CAN to send messages in APPBL. After powering off again, the CAN message cannot be received, and the entire controller is powered off.

    I am certain that the BOOT-SEQ bit is set.

 

0 Kudos
Reply
0 Replies