S32K3 SPD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 SPD

857件の閲覧回数
Neo1096
Contributor III

Hello.

I use RTD400 and SPD105, and the development board is the S32K312 144P development board

I added the uart module to the tested SPD module (including RAM and flash injection errors) program, and it worked normally. Then I added other modules. (Currently, only the DMA part has been tested, and adding only uart seems to be fine.) Without making any Settings, even if the header file is not referenced in the code, The program will also be in the function Clock_Ip_SetWaitStates(); Then it enters a hardware error interrupt.

I uploaded the code of the FCCU module without adding DMA, and it can run normally. However, after adding it, the clock initialization program hardware error occurs. What could be the reason for this and how can this problem be solved?

0 件の賞賛
返信
1 返信

829件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Neo1096

Please follow your duplicated question:

https://community.nxp.com/t5/S32K/S32K3-SPD-DMA/td-p/2121214

 

0 件の賞賛
返信