S32K3 Multilink(P&E) flash tool setting based on Design Studio 3.4.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 Multilink(P&E) flash tool setting based on Design Studio 3.4.

1,084 Views
StephenYeh
Contributor III

Hi Sir

We based on the S32K3 to implement bootloader & application FW.

Is there any setting that the Design Studio(3.4) don't erase all the flash region?

Or we can set the erase area by the advanced options.(ex: The following options is mute. )

 

StephenYeh_0-1669276167611.png

 

Tags (1)
0 Kudos
Reply
1 Reply

1,069 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

There are 3 possible memory ranges that you can set to keep intact. It actually erases all the blocks, putting back what was originally stored at these locations, which is the same thing as a result.

davidtosenovjan_0-1669645266209.png

 

 

0 Kudos
Reply