S32K3 Multilink(P&E) flash tool setting based on Design Studio 3.4.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K3 Multilink(P&E) flash tool setting based on Design Studio 3.4.

1,035 次查看
StephenYeh
Contributor III

Hi Sir

We based on the S32K3 to implement bootloader & application FW.

Is there any setting that the Design Studio(3.4) don't erase all the flash region?

Or we can set the erase area by the advanced options.(ex: The following options is mute. )

 

StephenYeh_0-1669276167611.png

 

标记 (1)
0 项奖励
回复
1 回复

1,020 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

There are 3 possible memory ranges that you can set to keep intact. It actually erases all the blocks, putting back what was originally stored at these locations, which is the same thing as a result.

davidtosenovjan_0-1669645266209.png

 

 

0 项奖励
回复