S32K3 How to setting FreeRtos with EB 29 for RTD2.0.0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 How to setting FreeRtos with EB 29 for RTD2.0.0?

Jump to solution
1,031 Views
wuxianlong
Contributor III

Hi, all 

    Where can i get more information?
untitled.png

DRs,
      xianlong

0 Kudos
Reply
1 Solution
1,012 Views
DanNguyenDuy
NXP Employee
NXP Employee

Hi xianlong,

This error is a bug of driver RTD_S32K3XX_2.0.0. This bug was raised with the ticket ID: ARTD-26627
It will be fixed in the next release.

Best regards,

Dan

View solution in original post

0 Kudos
Reply
4 Replies
1,013 Views
DanNguyenDuy
NXP Employee
NXP Employee

Hi xianlong,

This error is a bug of driver RTD_S32K3XX_2.0.0. This bug was raised with the ticket ID: ARTD-26627
It will be fixed in the next release.

Best regards,

Dan

0 Kudos
Reply
1,001 Views
wuxianlong
Contributor III

@DanNguyenDuy Hi,Dan

I have updated it to RTD2.0.1, but....

Will this bug affect the normal use of FreeRtos? If I ignore this error.

If so, is there a way to solve this problem?

BRs,

xianlong

0 Kudos
Reply
997 Views
DanNguyenDuy
NXP Employee
NXP Employee

Hi wuxianlong,

The RTD2.0.1 version still fixed this error not yet. At the moment, I saw that this error was fixed on the RTD_4.4_S32K396_3.0.0_CD01 and RTD_4.4_S32K358_3.0.0_CD01.

To solve this problem on the 2.0.0 version, you must select it is "OsIfBaremetalType" or "OsIfAutosarOsType"

Best regards,

Dan

0 Kudos
Reply
1,010 Views
wuxianlong
Contributor III

Hi,Dan

Thank you very much. This question has been bothering me for a long time.

Best regards,
xianlong

0 Kudos
Reply