S32K3 How to setting FreeRtos with EB 29 for RTD2.0.0?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 How to setting FreeRtos with EB 29 for RTD2.0.0?

ソリューションへジャンプ
2,150件の閲覧回数
wuxianlong
Contributor V

Hi, all 

    Where can i get more information?
untitled.png

DRs,
      xianlong

0 件の賞賛
返信
1 解決策
2,131件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hi xianlong,

This error is a bug of driver RTD_S32K3XX_2.0.0. This bug was raised with the ticket ID: ARTD-26627
It will be fixed in the next release.

Best regards,

Dan

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,132件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hi xianlong,

This error is a bug of driver RTD_S32K3XX_2.0.0. This bug was raised with the ticket ID: ARTD-26627
It will be fixed in the next release.

Best regards,

Dan

0 件の賞賛
返信
2,120件の閲覧回数
wuxianlong
Contributor V

@DanNguyenDuy Hi,Dan

I have updated it to RTD2.0.1, but....

Will this bug affect the normal use of FreeRtos? If I ignore this error.

If so, is there a way to solve this problem?

BRs,

xianlong

0 件の賞賛
返信
2,116件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hi wuxianlong,

The RTD2.0.1 version still fixed this error not yet. At the moment, I saw that this error was fixed on the RTD_4.4_S32K396_3.0.0_CD01 and RTD_4.4_S32K358_3.0.0_CD01.

To solve this problem on the 2.0.0 version, you must select it is "OsIfBaremetalType" or "OsIfAutosarOsType"

Best regards,

Dan

0 件の賞賛
返信
2,129件の閲覧回数
wuxianlong
Contributor V

Hi,Dan

Thank you very much. This question has been bothering me for a long time.

Best regards,
xianlong

0 件の賞賛
返信