S32K3: Hard Fault Error occurred, If the ISR execution time is more than 65us /100us

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3: Hard Fault Error occurred, If the ISR execution time is more than 65us /100us

1,354 Views
nkarthik
Contributor III

Hi NXP team,

 We are facing the S32K3: Hard Fault Error occurred, If the ISR execution time is more than 65us.

ISR Period is 100us.Please find attached document for more details.

Thanks&Regards

Karthik.N

0 Kudos
Reply
3 Replies

1,317 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Karthik,

There seems to be a couple of issues.

First of all, is the exception caused by the MPU?
In the exception handler, if you read the Configurable Fault Status Register (CFSR[MMFSR]), which of the errors do you see there?

https://developer.arm.com/documentation/107706/0100/System-exceptions/Fault-exceptions-and-their-cau...

I see you configure the MPU in the application using RTD MCAL.
Is the MPU configured in the startup code too, or is the MPU disabled there?

Thank you,

Best regards,
Daniel

 

 

0 Kudos
Reply

1,271 Views
nkarthik
Contributor III

hi ,

1.The issue is not caused by MPU.MPU is disabled both in Startup and Platform.

2.CFSR Register is 0x0

Please let me know if any other possible cause for this issue.

 

0 Kudos
Reply

1,247 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @nkarthik,

You said that you see Hard Fault exception there.

So, in the handler, you should see the type of the exception in CFSR.

Refer to these documents:

 

https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-HARDFAULT-Handling-Interrupt-DS3-5-...

https://community.nxp.com/t5/S32K-Knowledge-Base/How-To-Debug-A-Fault-Exception-On-ARM-Cortex-M-V7M-...

https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447


The stack corruption can be caused by by several reasons, for example:

  • Insufficient stack size,
  • Access to unimplemented memory,
  • Invalid pointers,
  • Unaligned memory accesses or MPU misconfiguration,
  • Cache coherency

 

Recomended debugging:

  • Analyze the fault exception.
  • Check stack usage - for example by initializing the SRAM with a known pattern that gets overwritten.
  • Increase the Stack size
  • Try with Cache disabled
  • Check the MPU configuration - It is importatnt to know exactly what are the attribites of each region.
  • Review interrupt priority
  • Review the errata: https://www.nxp.com/webapp/Download?colCode=S32K342_0P97C

 

Regards,

Daniel

 

 

 

 

0 Kudos
Reply