S32K1xx LPSPI 4-wire Swapping SIN/SOUT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K1xx LPSPI 4-wire Swapping SIN/SOUT

697 Views
Daniel_Wax
NXP Employee
NXP Employee

I’m interested if the HW peripheral supports using 4 wire SPI with the SOUT as input and SIN as output.

 

This seems to be the case according the reference manual.

Daniel_Wax_0-1600459033096.png

Daniel_Wax_1-1600459169354.png

 

Can you confirm internally that the HW peripheral supports 4 wire SPI with SIN and SOUT “swapped”.

 

Of course the master and slaves on each side will have to be reconfigured and swapped as master/slave.  Im just wondering if this enables swapping of ins for outs so one can change which side is master and which side is slave in the future if needed.

 

0 Kudos
0 Replies