[S32K1xx]About the parameter changed for the external OSC in the DS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[S32K1xx]About the parameter changed for the external OSC in the DS

658 次查看
GavinLi1
Contributor III

Dear Experts,

The max value of VIL for the external OSC changed from "0.35*VDD" to "1.15" in the DS(Rev.6 to Rev.14).

Why do the change, any considerations?

It seems that using the VDD=3.3V to get the max VIL, that is 0.35 * 3.3 = 1.15V.

But,

as we know, the S32K1xx works between 2.7~5.5V, so the 1.15 is rather strict when VDD= 2.7V, but relatively loose when VDD= 5.5V.

This is where I'm confused. Why is the MAX VIL wroten  as a fixed value 1.15 in the DS?

 

BR,

Gavin

0 项奖励
回复
2 回复数

653 次查看
GavinLi1
Contributor III

GavinLi1_0-1730945586284.png

Rev.6

GavinLi1_1-1730945603149.png

Rev.14

0 项奖励
回复

493 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @GavinLi1,

I'm trying to find the reason behind the change,

 

Regards,

Daniel

0 项奖励
回复