Hi there,
I have created a project with "S32DS Application project" button, over the S32k188 micro controller; it just a blinking led. Works fine debugging with the Mutilink Universal debugger; BUT I unplug this debugger and after a reset the led is fix to OFF. Seems that the microcontroller doesn't start to run. I have set the optimization to "None".
I have tried a "S32DS Project from example" button (hello_world_s32k118) and adding the blinking led code; and works fine with and without debugger!!!!!!
There is something different inside the project parameters, between the example and the application. I have compared them and matched some parameters, but with the same results.
IDE: S32 Design Studio for ARM Version: 2.2 Build id: 200116
Where I could be failing?
thanks a lot
已解决! 转到解答。
understood, done and running!!!!!
Bravo for you, and bravo for the NXPCommunity.
Thanks a lot
Hi albertgalofre,
Please add "START_FROM_FLASH" Symbols in "Standard S32DS Assembler".
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Robin.
I'm trying to solve same problem. but I can't see the tap that you let me see.
I think that's because I have another version S32DS.
I have S32 Design Studio for S32 Platform
- Version: 3.3
- Build id: 200610
I want to execute S32K188 without debugger.
What can I do?
Please see the discussion here: If I don't give s32k312 delay, the CAN stop during operation
If the problem is still not solved, it is recommended to click ASK A QUESTION in the S32K community.