S32K188 runs with debugger, but not witout

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K188 runs with debugger, but not witout

跳至解决方案
7,407 次查看
albertgalofre
Contributor II

Hi there,

I have created a project with "S32DS Application project" button, over the S32k188 micro controller; it just a blinking led. Works fine debugging with the Mutilink Universal debugger; BUT I unplug this debugger and after a reset the led is fix to OFF. Seems that the microcontroller doesn't start to run. I have set the optimization to "None".

I have tried a "S32DS Project from example" button (hello_world_s32k118) and adding the blinking led code; and works fine with and without debugger!!!!!!

There is something different inside the project parameters, between the example and the application. I have compared them and matched some parameters, but with the same results.

IDE:   S32 Design Studio for ARM        Version: 2.2     Build id: 200116

 

Where I could be failing? 

 

thanks a lot

 

标记 (3)
0 项奖励
回复
1 解答
7,379 次查看
albertgalofre
Contributor II

understood, done and running!!!!!

Bravo for you, and bravo for the NXPCommunity.

Thanks a lot

在原帖中查看解决方案

0 项奖励
回复
8 回复数
7,380 次查看
albertgalofre
Contributor II

understood, done and running!!!!!

Bravo for you, and bravo for the NXPCommunity.

Thanks a lot

0 项奖励
回复
7,395 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi albertgalofre,

Please add "START_FROM_FLASH" Symbols in "Standard S32DS Assembler".

START_FROM_FLASH Standard S32DS Assembler Symbols.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

4,395 次查看
binZhang01
Contributor III

I followed your instructions, but it didn't work. I am using the routine of S32K312

binZhang01_0-1715130891904.png

binZhang01_2-1715130935851.png

 

7,340 次查看
종찬박
Contributor II

Hi Robin.

I'm trying to solve same problem. but I can't see the tap that you let me see.

I think that's because I have another version S32DS.

I have S32 Design Studio for S32 Platform
 - Version: 3.3
 - Build id: 200610

image.png

I want to execute S32K188 without debugger.

What can I do?

0 项奖励
回复
7,336 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Yes. There is a little different between S32DS 2.2 and 3.3.
You can open Standard S32DS Assembler -> Preprocessor and then add START_FROM_FLASH

START_FROM_FLASH S32 Design Studio for S32 Platform 3.3.png

4,134 次查看
Luxls
Contributor I
It does not work when I try this method to debug S32K312 EVB.
0 项奖励
回复
4,121 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Please see the discussion here: If I don't give s32k312 delay, the CAN stop during operation
If the problem is still not solved, it is recommended to click ASK A QUESTION in the S32K community.

0 项奖励
回复
7,326 次查看
종찬박
Contributor II

I'm afraid that it doesn't work.

I did already what you said so, but my board doesn't work.

when I control my board with debugger, it works well.

but, After power reset, it doesn't work.

0 项奖励
回复