S32K14x and S32K11x package markings nomenclature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K14x and S32K11x package markings nomenclature

1,235 Views
dawidbabula
Contributor II

Hello,

where can I find information about nomenclature of markings on the microcontroller package ?

Best Regards,

Dawid

Tags (1)
0 Kudos
Reply
2 Replies

1,133 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello,

 

Here's the information regarding the marking code:

  • LINE 2: Mask set revision
  • LINE 3: Date code

The marking itself is NXP Confidential so I cannot share more details

 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,133 Views
dawidbabula
Contributor II

Hello Victor, 

thanks a lot for response, it's very helpful. However for LQFP64 footprint, which I got , LINE 3 seems to be Mask set revision and not LINE 2. Anyway I've decoded Mask set revision, for my uC. 

Thanks a lot,

Dawid

0 Kudos
Reply