S32K14x_MCAL_4_2_RTM_104: How to use Gpt Chain Mode Features on LPIT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K14x_MCAL_4_2_RTM_104: How to use Gpt Chain Mode Features on LPIT

674 Views
ou_gangxun
Contributor II

I set two Gpt channels 0 and 1, using LPIT_CH0 and LPIT_CH1 respectively, and set the GptChainMode property of LPIT_CH1 to True. Only channel 0 is started on the application, and the timeout period is 1000us, but there is no change in LPIT_CH1, and the millisecond count cannot be realized.

0 Kudos
1 Reply

651 Views
hungnguyenphi
NXP Employee
NXP Employee

Hello @ou_gangxun ,

The channel 1 also need to be started on the application. Then the channel 1 's timer decrements on channel 0 's timeout pulse 

Best regards,

Hung

0 Kudos