S32K14x GPIO PAD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K14x GPIO PAD

Jump to solution
1,584 Views
lihui1
Contributor II

If GPIO used as input, has this resister there on the input circuit ?


It seems like input current will flow through this resistor as below

c529469d710b0b49e8d6bd11c765fb2.jpg

Tags (1)
0 Kudos
Reply
1 Solution
1,579 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it is correct. It is Hi-Z input.

View solution in original post

0 Kudos
Reply
2 Replies
1,580 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it is correct. It is Hi-Z input.

0 Kudos
Reply
1,576 Views
lihui1
Contributor II

OK,thank you!

0 Kudos
Reply
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----