S32K14x EVB For ISELED

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K14x EVB For ISELED

Jump to solution
590 Views
Bussign
Contributor I

Hi NXP:

        I want to replace the S32K144-Q100 MCU with a Part number from the ISELED list. Can I directly replace it with the K146 series? In other words, can I replace the S32K144-Q100 MCU with FS32K146UIT0VLLT or FS32K146ULT0VLLT? Similarly, can I replace the MCU in S32K146evb-Q144 with FS32K148UIT0VLQT or FS32K148UGT0VLQT?

Bussign_0-1690510419620.png

Thanks.

0 Kudos
Reply
1 Solution
561 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Q: Can I replace the S32K144-Q100 MCU with FS32K146UIT0VLLT or FS32K146ULT0VLLT?
Answer: Yes. you can.
But maybe you can ask for a sample FS32K144ULT0VLLT. Pay attention to use the company email address, and the number of samples should be less than 3 pieces.

FS32K144ULT0VLLT SAMPLE.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
562 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Q: Can I replace the S32K144-Q100 MCU with FS32K146UIT0VLLT or FS32K146ULT0VLLT?
Answer: Yes. you can.
But maybe you can ask for a sample FS32K144ULT0VLLT. Pay attention to use the company email address, and the number of samples should be less than 3 pieces.

FS32K144ULT0VLLT SAMPLE.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply