S32K148EVB issue with the part number of the MCU on the board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148EVB issue with the part number of the MCU on the board

ソリューションへジャンプ
569件の閲覧回数
Chris_Tigger
Contributor III

Hi,

I bought a S32K148EVB-Q176 several days ago,I have a question about the Ethernet part.

Chris_Tiger_0-1748041572394.png

the datasheet mentions that the S32K148UA series does not have Ethernet support,As shown in the picture above.Both the S32K148EVB-Q176 schematic and things are using the S32K148UA series, As shown in the figure below.So can my board use Ethernet?

Chris_Tiger_1-1748041792741.pngChris_Tiger_2-1748041838502.png

 

Best Regards!
Chris Tigger
タグ(2)
0 件の賞賛
返信
1 解決策
485件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you want to test ethernet, buy S32K148EVB-KIT version directly (https://www.nxp.com/part/S32K148EVB-KIT) as you will need ethernet PHY board as well.

BR,Petr

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
516件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I assume it is OK. Anyway you can read SIM_SDID register, bit 3 of FEATURE field should indicate presence of ENET module.

BR, Petr

0 件の賞賛
返信
506件の閲覧回数
Chris_Tigger
Contributor III
I am considering purchasing a version of the S32K148UJ. The board has been returned to the agent and is currently unavailable fot testing. but I am in mainland of China, it is most convenient to buy through an agent. Look at many,basically are S32K148UA or S32K148HA,it would be best if I could get an accurate answer here.
Best Regards!
Chris Tigger
0 件の賞賛
返信
486件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you want to test ethernet, buy S32K148EVB-KIT version directly (https://www.nxp.com/part/S32K148EVB-KIT) as you will need ethernet PHY board as well.

BR,Petr

0 件の賞賛
返信