S32K148EVB-Q176 debugging issue !

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K148EVB-Q176 debugging issue !

2,405 次查看
Saitej
Contributor IV

Hello NXP

Am with S32K148 with IDE S32 Design Studio. While am trying to debug with break points, cursor is not getting stopped at the break point. Observed threads got missed to track.

using on board debugger Open SDA

Please do the needfull.

Console Message:

Task name is Task_10ms
Task name is Task_2ms
Task name is Task_1ms
Number of threads 9 qfThreadInfoIterator: 0
Number of threads 9 qfThreadInfoIterator: 9
Number of threads 9 qfThreadInfoIterator: 0
Number of threads 9 qfThreadInfoIterator: 9
rsp_qThreadExtraInfo - Thread extra info grabbed - result: 5461736B5F31306D73
rsp_qThreadExtraInfo - Thread extra info grabbed - result: 5461736B5F316D73
rsp_qThreadExtraInfo - Thread extra info grabbed - result: 5461736B5F326D73
rsp_qThreadExtraInfo - Thread extra info grabbed - result: 5461736B5F356D73
rsp_qThreadExtraInfo - Thread extra info grabbed - result: 5461736B5F3130306D73
rsp_qThreadExtraInfo - Thread extra info grabbed - result: 49444C45
Number of threads 9 qfThreadInfoIterator: 0
Number of threads 9 qfThreadInfoIterator: 9

标记 (3)
0 项奖励
回复
5 回复数

2,381 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it could be caused by optimizations. I would check if the optimization level is set to 0:

lukaszadrapa_0-1617708487337.png

 

Regards,

Lukas

 

0 项奖励
回复

2,374 次查看
Saitej
Contributor IV

Hello @lukaszadrapa 

Thanks for the response 

Currently we have zero optimisation's, Am able to break it in few trials as it is random.

Saitej_0-1617711737105.png

 

0 项奖励
回复

2,347 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

is OS Awareness enabled like this?

lukaszadrapa_0-1617787919041.png

 

And if this doesn't help, is it possible to share the project, so we can try to reproduce the behavior on our side?

Thanks,

Lukas

 

0 项奖励
回复

2,333 次查看
Saitej
Contributor IV

Hello @lukaszadrapa 

Yes, OS awareness is enabled , it not helped us.

It's not possible to send the project , if you guide me will share all the logs with to debug the issue.

0 项奖励
回复

2,394 次查看
Saitej
Contributor IV

any help please

0 项奖励
回复